Loading
CASE STUDY | Pulp & Paper, Household & Personal Care
Recent ActivityRecent Activity

Encore Tissue Upgrades Plant Reliability with PlantPAx DCS

User-friendly software enhances productivity of key tissue manufacturing equipment

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Two boxes of Encore tissue icare
Encore Tissue Logo

Encore Tissue was born in 1998, when the Holckner Family purchased a small tissue business. Encore’s vision was clear from the beginning; to provide quality tissue product to the Australian market, whilst endeavouring to be socially, economically and environmentally sustainable.

Challenge
  • With production ramping up, Encore Tissue sought a modern DCS solution that would deliver productivity gains, offer a user-friendly interface, and include long-term support.
Solution
  • After thorough review, Encore Tissue selected PlantPAx® Distributed Control System (DCS) to replace the older solution.
Result
  • By implementing PlantPAx, Encore Tissue now has a unified system. A Rockwell DCS is communicating with a Rockwell safety controller, which controls the PowerFlex® drives. This simplifies integration with the drives system, as well as enabling simple upgrades in the future.

Encore Tissue, a leading Australian manufacturer of toilet paper and paper towels, has enhanced the efficiency and reliability of its Victorian plant by upgrading to Rockwell Automation’s PlantPAx® Distributed Control System (DCS).

Rockwell has worked with Encore Tissue – which produces household brands like icare toilet paper – for more than 20 years, first working on the tissue machine’s DC drive system in the early 2000s, then converting half to AC in 2014 and the other half in 2017. The AC drive system is based on Rockwell’s PowerFlex® 755. The upgrade of the tissue machine has enabled Encore Tissue to increase production output from the plant.

Encore Tissue is an Australian family-owned business with a vision to provide quality tissue product to the Australian market, whilst endeavouring to be socially, economically, and environmentally sustainable.

Challenge

With production ramping up, Encore Tissue sought a modern DCS solution that would deliver productivity gains, offer a user-friendly interface, and include long-term support.

Encore Tissue Machine

“Our existing DCS had become outdated, and was no longer supported,” said Mark Camilleri, project manager at Encore Tissue. “Rockwell has extensive knowledge of our machinery and plant through our long relationship, so we engaged them to look at upgrading our DCS.”

In addition to new functionality, Encore Tissue wanted the new DCS solution to have a user-friendly software interface that could be used by multiple teams.

Solution

After thorough review, Encore Tissue selected Rockwell Automation’s PlantPAx DCS to replace the older solution.

“PlantPAx is an open DCS, which means partner companies, such as system integrators with knowledge of the system, can provide support, too,” explains Adrian Giecco, regional director – South Pacific, Rockwell Automation.

Encore Rockwell Automation PlantPAX DCS

PlantPAx is a modern DCS that provides a single plant-wide control system to increase flexibility, boost efficiency, reduce costs, and enable better business decisions, for companies in pulp and paper, manufacturing, process engineering, mining and resources, food and beverage, water and wastewater and a broad range of industrial sectors.

“The PlantPAx software shares the same platform as the Rockwell drive system already in use at Encore Tissue, so their staff are already familiar with how to use it, which meant there was a smaller learning curve for the migration to PlantPAx,” said Giecco.

Encore Rack 5

The new PlantPAx solution (hardware pictured), uses the same software platform as existing Rockwell drives, so staff are already familiar with many of its functions

To allow for a smooth transition, Rockwell was able to extract the code and logic configuration from the existing DCS and re-map it to PlantPAx logic, thereby ensuring object alarms, limits, tuning, references, and other setups remained the same without the need to re-commission or re-tune.

“This is a proven approach to quickly migrate the process functionality to the PlantPAx standard and minimise risk,” said Giecco.

“Another way Rockwell minimised risk on this project was by re-using existing wiring. The existing control systems use Allen-Bradley® ControlLogix® hardware and, as such, the I/O modules can be replaced as a ‘like-for-like’ system while keeping the existing terminal modules and wiring looms intact, significantly reducing risk of migration and reducing commissioning time.”

Result

By implementing PlantPAx, Encore Tissue now has a unified system. A Rockwell DCS is communicating with a Rockwell safety controller, which controls the PowerFlex drives. This simplifies integration with the drives system, as well as enabling simple upgrades in the future.

“We needed to upgrade the hardware due to its age, so selecting Rockwell meant we were given better support from a company with dedicated and proven process automation experience,” said Camilleri.

“Encore Tissue also takes care of critical spares via the Rockwell Automation Inventory Parts Management Agreement,” he said.

The new system also reduces the physical footprint, requiring only two controllers instead of four and occupying less panel space.

“PlantPAx is also designed to allow manufacturers like Encore Tissue to more simply and efficiently follow industry standards and best practices,” said Giecco.

To make commissioning and startup as smooth as possible, Rockwell undertook an extensive Factory Acceptance Testing (FAT) period of several weeks.

“FAT is usually just a couple of days, but we wanted everything to run smoothly for Encore Tissue, so we went into meticulous detail with our testing,” said Giecco.

“As a result, the entire migration – from the start of commissioning to production – was completed in just four days, making it a highly efficient transition.”

“The steps that needed to be taken while the machine was offline were all completed within a 72-hour window from paper off to paper on, thereby achieving a successful result in a tight window.”

Published August 18, 2025

Topics: Optimize Production Production Automation Process Solutions Pulp & Paper Household & Personal Care PlantPAx
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies
  5. Chevron LeftChevron Left Encore Tissue Upgrades Plant Reliability with PlantPAx DCS