General Features
This application uses a virtual axis as a master so the correction movements between the axes InFeed and Knife become independent from each other.
General Features
This application uses a virtual axis as a master so the correction movements between the axes InFeed and Knife become independent from each other.
Advangages
Downloads
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
This application can be used in cutting-on-the-fly machines, horizontal packaging, or any other type of application where an electronic cam with position correction is required. The application can be used as a complement to some existing code libraries.
How can I make it work?
Hardware
Software
Prior Knowledge
Once we have made the adjustments for both Master” and Cam Lock Positions, we can now set up the Knife Phase Correction routine.
For this a “Motion Arm Registratio” instruction is used to record the knife position at the time of detection of the Registration Mark.
In this instruction the registration mark detection window can be adjusted if it is necessary to discriminate detections outside the appropriate position range.
Phase Correction in Cutting for Horizontal Balers
Version 2.0 - September 2026