Downloads
What does this application do?
The raDK_Tec_ShiftRegisterAxis Add-On Instruction (AOI) monitors and tracks product data as items move through a production line, conveyor, or similar axis-based transport system. The AOI uses the current axis position together with a configured work-area size and unwind position to shift data through an array of defined positions. New product data can be inserted at the beginning of the register, carried through the process, and made available at the output when it reaches the end. The application is intended as a reusable Studio 5000 building block that can be integrated into a machine program. It supports automatic item and shift-register identification, entry and exit timestamps, user-defined data, reset control, readiness indications, modulo position, and calculated pitch. The reference material does not specify supported controller families, Studio 5000 versions, firmware revisions, or production validation requirements; these must be confirmed for the target machine before deployment.
- Purpose: Provide a reusable method for synchronizing product information with physical axis movement.
- Context: Intended for production lines, conveyors, and similar transport mechanisms where products must be tracked through known positions.
- Objective: Maintain accurate item data and position tracking so downstream automation can handle each product at the correct point in the process.
- Use Mode: Used as a single AOI integrated into a Studio 5000 machine application.
- Problems Addressed: Reduces custom shift-register logic and helps keep product data aligned with axis positions across a defined work area.
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Is this application relevant to me?
- Benefits
- Advantages
- Limitations
- Considerations
- Tracks product information through defined physical positions.
- Stores automatically generated item IDs, shift-register IDs, entry times, exit times, and user data.
- Reusable single-AOI implementation.
- Pitch is calculated from the configured work-area size and array size.
- Provides status, modulo-position, reset, and diagnostic outputs through a consistent interface.
- The shift-register array must contain at least two elements. Cfg_AreaSize and Cfg_Unwind must be greater than zero, and Cfg_Unwind must not be smaller than Cfg_AreaSize. Hardware, software, and firmware compatibility are not defined in the source material.
- Requires a valid axis-position input and correct unwind configuration.
- User data must be structured using raDK_UDT_ShiftRegister_UserData.
- Incorrect area or unwind values stop correct operation and produce an error code.
- Machine-specific safety, recovery, and production validation remain the implementer’s responsibility.
How can I make it work?
Requirements: products, tools, prior knowledge.
The following requirements are based on the available application presentation.
Exact catalog numbers, software versions, controller firmware, and import packages are not stated and must be verified before implementation.
Hardware
- Control or Compact Logix controller
Software
- Studio 5000 Logix Designer V36 or newer
- PowerPoint