I/O Modules

A redundancy system supports I/O modules in a remote chassis. You cannot use I/O modules in a redundant chassis.
Without bridging, only the
EtherNet/IP
network is supported between a redundant chassis and remote I/O chassis.

Supported Products

You can use the following I/O products in a remote chassis that is connected to a redundant chassis pair:
  • 5034
    PointMax®
    I/O
  • 5094
    FLEX 5000®
    safety I/O (Logix SIS only)
  • 5094
    FLEX 5000®
    I/O
  • 5015
    FLEXHA 5000
    I/O
  • 1756
    ControlLogix®
    I/O
  • 1715 Redundant I/O
  • 1794
    FLEX I/O
  • 1734
    POINT I/O
This is not a complete list of supported I/O products and some restrictions exist. For more information, see the Knowledgebase Technote .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal