Update the Redundancy Module Firmware in the Primary Chassis

To update the redundancy module firmware in the primary chassis, complete these steps.
  1. Launch
    ControlFLASH Plus®
    software.
  2. Update the redundancy module firmware.
  3. Once the firmware update is complete, verify that the redundancy module status displays PRIM, which indicates a successful upgrade.
  4. Close the
    ControlFLASH Plus®
    software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal