EDS Files
If you see modules that are displayed in
FactoryTalk® Linx
software with yellow question marks, the EDS files for the modules are not registered. You can right-click the module and use the wizard to upload the EDS file. If this option is not available or as an alternative, follow this link to obtain the EDS files for modules in your system:
- Download the required EDS file.
- Select Start > Programs > Rockwell Software > EDS Hardware Installation Tool.The tool prompts you to Add or Remove EDS files.
Your redundant system firmware update is now complete.
Provide Feedback