Track Changes to Components
In the
Studio 5000 Logix Designer®
application, you track whether routines, Add-On Instructions, and constant tags have been changed. The Logix Designer application creates a tracked state value to indicate the current state of all components. Tracked components appear in the Tracked Components dialog box, which is accessible from the Security tab of the controller properties.
For more information, see the Logix 5000 Controllers Information and Status Programming Manual, publication 1756-PM015.
Provide Feedback