Reset an IP Address
You can reset the IP address of an
EtherNet/IP™
communication module to the factory default value. To return to the factory default, follow these steps.- Set the rotary switches on the module to 888.
- Restart the communication module.
- Set the switches on the module to the desired address or set the switches to 999.
Provide Feedback