Parallel Redundancy Protocol (PRP)

Parallel Redundancy Protocol (PRP) is defined in international standard IEC 62439-3 and provides high-availability in Ethernet networks. PRP technology creates seamless redundancy by sending duplicate frames to two independent network infrastructures, which are known as LAN A and LAN B.
A PRP network includes the following components.
PRP Components
Component
Description
LAN A and LAN B
Redundant, active Ethernet networks that operate in parallel.
Double attached node (DAN)
An end device with PRP technology that connects to both LAN A and LAN B.
Single attached node (SAN)
An end device without PRP technology that connects to either LAN A or LAN B. A SAN does not have PRP redundancy.
Redundancy box (RedBox)
A switch with PRP technology that connects devices without PRP technology to LAN A and LAN B.
Virtual double attached node (VDAN)
An end device without PRP technology that connects to both LAN A and LAN B through a RedBox.
A VDAN has PRP redundancy and appears to other nodes in the network as a DAN.
Infrastructure switch
A switch that connects to either LAN A or LAN B and is not configured as a RedBox.
For more information about PRP, see the EtherNet/IP Parallel Redundancy Protocol Application Technique, publication ENET-AT006.

Use PRP in a Redundancy System

For supported PRP I/O network topologies and design guidelines for high availability systems, see the High Availability Systems Reference Manual, HIGHAV-RM002.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal