EtherNet/IP Indicators
The EtherNet/IP status indicators show the state of the EtherNet/IP port and communication activity.
Indicator | State | Description |
|---|---|---|
NET | Off |
|
Flashing green | The controller has an IP address, but no active connections are established. | |
Steady green | The controller has an IP address and at least one established active connection. | |
Steady red | Duplicate IP address or invalid configuration. | |
LINK | Off | No activity. One of these conditions exists:
|
Flashing green | All of these conditions exist:
| |
Steady green | On a single-port controller, a link exists on the port, but no traffic is being received. On a dual-port controller, all of these conditions exist:
|
Provide Feedback