Routable CIP Safety System

The following example illustrates the extent of a routable
CIP Safety
system. In this example, the system is not interconnected to another
CIP Safety
system through a larger, plant-wide Ethernet backbone.
Routable CIP Safety System
Routable CIP Safety System
Item
Description
A
For a backplane port, an SNN is assigned to the backplane and the node address is the slot number of the device.
B
For an Ethernet port, an SNN is assigned to the
EtherNet/IP
network and the node address is the IP address of the device.
C
For a controller in Dual-IP mode and connected to two separate
EtherNet/IP
networks, they must not share SNN values because the switches can incorrectly route packets between them.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal