Controller Ethernet Port

You can disable a controller Ethernet port with the
Studio 5000 Logix Designer®
application.
IMPORTANT:
Remember the following:
  • For controllers with two Ethernet ports, you can disable either of the Ethernet ports whether the controller uses Dual-IP mode or Linear/DLR mode.
  • Once a port is disabled, you lose any connection that is established through the controller Ethernet port.
  • You cannot disable Ethernet ports if the controller switch is in Run mode or if the
    FactoryTalk® Security
    settings deny this editing option.
Ethernet ports return to the default setting after one of these actions occurs on the controller:
  • Stage 1 reset
  • Stage 2 reset
  • New project is downloaded - In this case, the settings in the new project take effect.
  • Program is cleared from the controller - These examples clear the program from a controller:
    • Major nonrecoverable fault occurs.
    • Firmware update occurs.
You must reconfigure the settings to disable an Ethernet port after the port returns to its default settings.
There are two ways to disable an Ethernet port:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal