Manual Assignment of Safety Network Number

Manual assignment is useful if you lay out your network and put the SNNs on your network diagram. It may be easier to read SNNs from a diagram than it is to copy and paste them from multiple projects.
Manual assignment of the SNN is required if the following is true:
  • One or more controller ports are on a
    CIP Safety
    subnet that already has an established SNN.
  • A safety project is copied to another hardware installation within the same routable
    CIP
    Safety system.
IMPORTANT:
If you assign an SNN automatically or manually, make sure that system expansion does not result in a duplication of SNN and unique node reference combinations.
A warning appears if your project contains duplicate SNN and unique node reference combinations. You can still verify the project, but Rockwell Automation recommends that you resolve the duplicate combinations.
However, there can be safety devices on the routable safety network that have the same SNN and node address and are not in the project. In this case, these safety devices are unknown to the Logix Designer application, and you will not see a warning.
If two different devices have the same node references, the safety system cannot detect a packet received by one device that was intended for the other device.
If there are duplicate unique node references, as the system user, you are responsible for proving that an unsafe condition cannot result.
Follow these steps to change the controller SNNs to manual assignments.
  1. On the Online toolbar, click the Controller Properties icon.
  2. On the Controller Properties dialog box, click the Safety tab.
  3. On the Safety tab, click the ellipse button to the right of the safety network number for the port that you want to change.
    This image shows where to click the ellipse for a SNN on the ControlLogix 5590 Properties dialog box in Logix Designer.
  4. On the Safety Network Number dialog box, select Manual.
  5. Enter the SNN as a value from 1…9999 (decimal) and then click OK.
    This image shows where to configure an SNN to the manual format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal