Use ControlFLASH Plus Software to Update Firmware

Use
ControlFLASH Plus®
software to flash firmware revisions on one or more devices. You browse to the devices from the Flash Devices tab and select the network path.
  • Click Select a Browsing Path button to set up the browsing path on the network.
  • If a path is already established, click Select Browsing from Path.
This image shows where to click in ControlFLASH Plus to start browsing.
The network browser shows the devices in your system.
The following steps show how to select devices and firmware.
  1. In
    ControlFLASH Plus®
    software, select the device, select the firmware revision as shown in the following example, and click Next to confirm.
    This image shows where to select the device and desired firmware revision in ControlFLASH Plus.
    If a firmware revision needs to be downloaded from the Product Compatibility and Download Center, the Download Center License Agreement dialog box opens, and you follow the prompts to download the firmware revision.
  2. If the updated screen shows the correct selections, click Flash.
  3. When a dialog box prompts you to confirm whether to trust the publisher of a DMK during the update, you must trust it to continue. 
  4. When the operation completes, click Close.
    If necessary, click Retry to flash devices whose flash operations have failed or were canceled.
    NOTE: For more details on how to use
    ControlFLASH Plus®
    , see the online help or ControlFLASH Plus Quick Start, CFP-QS001
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal