Connect the Supplemental Power Tap

  1. Insert the 1486-CON connector with the attached 1486-CON flat cable media into the connection jack on the power tap.
    TIP:
    For a 1486-CON-P2L connector, make sure the etched arrow and cable are positioned left to right.
    For a 1486-CON-P2R connector, make sure the etched arrow and cable are positioned right to left.
    Connect the Supplemental Power Tap
    A supplemental power tap with flat cables
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal