Reseat the Communication Interface Module on a Push Button
- If the latch is not properly seated on the operator/panel, insert a small flathead screwdriver into the latch collar
, then rotate the latch collar to the right
.
Applying pressure by hand is also an option to rotate the latch collar if a small flathead screwdriver is not available. - To reseat the communication interface module, remove the latch with the module from the 800F operator.
- Insert a small flathead screwdriver into the lever
on the bottom of the communication interface module.
- Gently pry the lever down until the communication interface module is released from the mounting latch of the 800F operator.
- Follow the steps in Connect an 800F Operator to the 800F Communication Interface Module to reinstall the module.Reseat Communication Module on Push ButtonItemDescriptionLatch collarRotate the latch collarLever
Provide Feedback