DIN Rail Mount the Gateway

  1. Pull each mounting clip away from the DIN rail as shown.
    IMPORTANT:
    Secure the DIN rail to a mounting surface approximately every 20 cm (7.87 in.) and use end-anchors appropriately.
    DIN Rail-mounted Gateway (shown from rear)
    An Ethernet gateway mounted onto a DIN rail
  2. Place the gateway onto the DIN rail (TH35 per IEC 60715).
  3. Push each mounting clip toward the DIN rail.
  4. Use end anchors next to the left and right sides of the gateway to lock it into place on the DIN rail.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal