Automatic Device Configuration
Automatic Device Configuration (ADC) helps to reduce downtime in a field replacement situation by automatically downloading the configuration rather than manually with a separate tool. With ADC enabled, the controller automatically downloads the configuration settings for the device.
ADC is always enabled in the gateway and the end node devices. With ADC, the controller
automatically downloads the configuration settings for the gateway and connected end node
devices each time the controller connects to the gateway.
Provide Feedback