Corrected anomalies
This list identifies the anomalies that are corrected in the Logix Designer application
version 38.02. Use the identification information provided in parentheses to track the anomaly
in future releases or for reference when receiving assistance from Customer Support with a
related issue.
General
Polish special character cannot be added (4004303, 5389622)
Using a keyboard to add the Polish character “ą” in the Tag Description popup selects all
text in the popup box. The character can be typed in other Tag Description fields.
This anomaly corrected in Logix Designer version 38.02.
This anomaly first identified in Logix Designer version 33.00.
Slow online performance of Logix Designer (5518773, 5604261)
Studio 5000 Logix Designer software may experience delays in response or go completely
unresponsive as more routines are open. This is more likely to occur with routines that
reference a large number of tags in 5370 and 5570 Controller applications.
This anomaly corrected in version 38.02.
This anomaly first identified in version 37.00
Online editing of CMP or CPT instructions takes the application offline (5410979,
5505436)
Online editing of Compare (CMP) or Compute (CPT) instructions causes the application to go
offline with the following error:
Failed to correlate the project with a change in the controller. Logix Designer has been
taken offline. Error 727-0.
The anomaly occurs if the instruction expression includes:
- A tag of a user-defined data type (UDT) array using indirect addressing.
- A large, nested UDT array member.
- A comparison or compute to a tag or tag expression.
For more information, see technote BF33114 - Studio 5000 Logix Designer: Communication Error
727-0 when online editing of Compare (CMP) or Compute (CPT)
This anomaly corrected in version 38.02.
This anomaly first identified in version 38.00.
SFC routine actions not executed correctly with aliased steps (5724850, 5644652)
An SFC routine does not execute actions as expected when steps use
aliased backing tags. For example, the active action displayed in the editor may belong to the
previous step, even though the code has executed. To resolve this, remove alias parameters
from SFC_STEP backing tags.
This anomaly corrected in version 38.02.
This anomaly first identified in version 38.00.
ControlNet network requires rescheduling after downloading unchanged project (5104247,
5434785)
The ControlNet network requires rescheduling when downloading an
unchanged project.
To resolve this, select
File
> Save
and merge changes into the existing
schedule.This anomaly corrected in version 38.02.
This anomaly first identified in version 37.00.
Provide Feedback