Backing Tag Properties dialog box - Parameters tab overview
Use the
Parameters
tab of the Backing Tag Properties
dialog box to get an
overview of all the parameters associated with the selected Function Generator (FGEN)
instruction.
TIP:
- Function Block: To open theBacking Tag PropertiesdialogParameterstab, right-click the instruction and selectProperties.
- Ladder Diagram: To open theBacking Tag Propertiesdialog , select the configuration icon.
Provide Feedback