Comment Text Block command

Select the
Comment Text Block
command to add comment text. Additionally, use the
Comment Text Block
command to:
  • Mark the entire selection as a multi-line comment.
  • Add a single line comment to the line that contains the cursor when no text is selected.
  • Add "//" comment delimiter to the beginning of each line when using line selection to select individual lines.
  • Add "(*" and "*)" delimiters to the beginning and the end of the text selection, respectively, when selecting a portion of text that spans multiple lines, either entire lines or portions of them.
    TIP:
    Comments in structured text routines are downloaded into the controller with routine logic. Start a pending edit to edit them online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal