PPID setpoint source and clamping limits
Use the
SP
tab on the PPID Properties
dialog box to monitor the source and processing of the setpoint value and to configure the setpoint clamping limits for Process Proportional + Integral + Derivative (PPID) instructions.To monitor the setpoint source and configure setpoint clamping limits
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theGeneraltab, select theSPtab.
- In theOperator Setpoint/Ratio valuebox, enter or monitor the setpoint (SP) or ratio value from the operator. This parameter is used for the ratio value when the loop mode is configured asCascadeand the instruction is configured forRatio. If the setting requires a signature, this will enforce security from the HMI and disable the setting from the Logix Designer dialog.NOTE: Use theHMItab to assign a unit label for the SP units on this tab.
- In theSP clamping limitsboxes, enter the high and low clamping limits. Use this numerical entry to check or set the high and low limit value at which the SP is clamped.
- Monitor these parameters:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state, suchSP rampingorCV held.
- Device issues. When theLogix Designerapplication is online with the controller, displays fault conditions, such asPV uncertain,SP fail, orConfiguration error.
- Device mode. When theLogix Designerapplication is online with the controller, displays the current device mode:
- Manual
- Auto
- Cascade (no Ratio)
- Ratio
- Program Setpoint/Ratio value. Displays the Program defined setpoint or ratio value. This parameter is used for the ratio value when the loop mode is configured asCascadeand the instruction is configured forRatio.
- External Setpoint/Ratio value. Displays the Externally defined setpoint or ratio value. This parameter is used for the ratio value when the loop mode is configured asCascadeand the instruction is configured forRatio.
- Override Setpoint/Ratio value. Displays the setpoint or ratio value supplied in Override. This parameter is used for the ratio value when the loop mode is configured asCascadeand the instruction is configured forRatio.
- SP ramp wizard. Displays the status of Setpoint ramp wizard function. The ramp wizard function can be in progress, enabled, or disabled. Ramping is not available when the instruction is configured forRatio.Use theAdvancedtab to enable the ramp wizard. Use theSP ramptab to enter target ramp values and to start and stop ramping.
- Current ratio. Displays the actual ratio value from the in-service source after clamping.
- Cascade SP. Displays the actual value from Inp_CascSP. When the loop mode is set toCascade, this input is a setpoint from the outer loop. When the loop mode is set toCascadeand the instruction is configured forRatio, this input is a process variable.
- Current SP rate of change limits. Displays the SP rate-of-change limits. Use theAdvanced > Limitstab to set the SP rate-of-change limits. The limit values can either be configured on theLimitstab or can be calculated by the SP ramp wizard when the wizard starts.
- Current PV. Displays the value from Inp_PV which is used as a setpoint if the original SP cannot be used and the instruction is configured for this shed. Use theAdvancedtab and theAdvanced > Loopmode tab to configure the conditions that trigger SP by PV replacement.
- Interlock SP. Displays the value from Cfg_SPIntlk which is used as a setpoint if the original SP cannot be used and the instruction is configured for this shed in interlock. Use theAdvanced > Loopmode tab to configure the conditions that trigger SP by PV replacement.
- Target for SP. Displays the target SP value before ramping.
- Current SP. Displays the SP value after ramping, Val_SP. Val_SP provides SP value to the PID formula.
- SelectApply.
Provide Feedback