HMI navigation for PDBC
Use the
HMI Navigation
tab on the PDBC Properties
dialog box to enable or disable navigation from the HMI to input and output objects.To enable HMI navigation to input and output objects for Process Deadband Controller (PDBC) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to the input and output object from the HMI faceplate, selectAllow navigation.
- In theObject tag namebox, enter the path to the object.
- When online with the controller, monitor theDevice state,Device issues, andDevice modeindicators at the bottom left of the dialog box:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state:
- Deadband, Q is off
- Deadband, Q is on
- Above Lower setpoint
- Below Raise setpoint
- Same in manual
- Out of service
- Device issues. When theLogix Designerapplication is online with the controller, displays fault status:
- None
- Low deviation
- High deviation
- High rate of change (decreasing)
- High rate of change (increasing)
- Input source bad
- Configuration error
- Device mode. When theLogix Designerapplication is online with the controller, displays the current device mode:
- Auto
- Manual
- Normal
- SelectApply.
Provide Feedback