Import/Paste Configuration dialog box - Configure Connections tab
Use this dialog box to configure connections when importing/pasting a program into a project.
TIP:
To open the Import/Paste Configuration dialog - Configure Connections tab:
- ClickFile > Import Component > <component>.
- Select a component for import and clickOpen.
- On theImport Contentpane, clickConnections.
In this dialog box, configure connections to program parameters or controller scope tags that exist in the project. When importing a program or programs and the import operation for the program(s) is set to
Create
or Overwrite
, connections can be configured in the Connections
grid. Otherwise, if the import operation is set to Use Existing
or Discard
, the Connections
grid will not be present.The leftmost part of the grid provides an indication of the condition of the connection.
* | Indicates a row where content has changed and the change has not been saved. |
Indicates a row in which the connection endpoints are invalid due to a syntax error. When select OK to begin the import, an error message shows. Fix or remove the connection before proceeding. | |
![]() | Indicates that the connection being imported will contain an error at the completion of the import. Proceed with the import, and the connection is created, but fix the error before downloading the project to the controller. |
Indicates a row to create a connection. |
Provide Feedback