Configure sequencing parameters
Configure the that can be configured.
Value
and Initial Value
on sequencing input parameters and Initialize As Valid
and Expression
attributes on sequencing output parameters. Both types of sequencing parameters have a Description
attribute
TIP:
To quickly find sequencing parameters in the Sequence Tag Editor, use the
Show
list to select the Sequencing Parameters
option.To configure sequencing parameters:
- In the Sequence Tag Editor, find the sequencing input parameter or sequencing output parameter to configure.
- Select the sequencing input parameter and do these steps:
- (Optional) Enter a value inInitial Value.
- (Optional) Enter a value inValue.
- (Optional) Enter text inDescription.
- Select a sequencing output parameter and do these steps:
- (Optional) Enter a value inInitial Value.
- (Optional) SelectInitialize as Validas needed.
- Enter an expression inExpression.
- (Optional) Enter text inDescription.
Provide Feedback