About component tracking
Use component tracking to determine whether tracked components have been changed. The
Logix Designer
application creates an overall tracked value to indicate the current state of tracked components.Tracked components and their current states appear in the Tracked Components dialog box, which is accessible on the Controller Properties dialog box - Security tab. The following components can be tracked:
- Routines
- Add-On Instructions
- I/O Modules
- Constant tags
Recommended limits for tracked components
The following table lists the recommended limits on the number of components that can be tracked. If the limits are exceeded, there might be a noticeable impact on performance in the
Logix Designer
application.
TIP:
To optimize performance, configure component tracking so that the tracked state value is calculated on demand rather than at regular intervals.
Tracked component | Recommended limit |
Routines | 100 |
Add-On Instructions | 100 |
I/O Modules | 50 |
Tags | 300 |
FactoryTalk Security
permissions that control component trackingThe following
FactoryTalk Security
permissions control a user's ability to change tracking status for a component:- Routine: Modify Properties
- Add-On Instruction: Modify
- Module: Modify Properties
- Tag: Modify Properties
Provide Feedback