Actions page

Use the
Actions
page to:
  • Configure how an axis responds to fault types.
  • Modify actions for how an axis responds to fault types.
    TIP:
    Some of the options for each of the actions, such as the options for the
    Disable (MSF) Stopping Action
    control, may change depending on the axis configuration and information from the drive's profile.
TIP: To open the Actions page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    Actions
    .
The parameters are separated into Standard Actions and Safety Actions.
Standard Actions parameters
Parameter
Description
Disable (MFS) Stopping Action
Select the stop action for the motor.
The options vary depending on the axis configuration type selected on the
General
page.
If the
Axis Configuration
on the
General
page is set to:
  • Feedback only
    - This field appears dimmed and retains the value of its last state.
  • Frequency Control - Valid values include:
    • Disable & Coast
    • Current Decel & Disable
    • Ramped Decel & Disable
    • Current Decel & Hold
    • Ramped Decel & Hold
    • DC injection brake
    • AC injection brake
  • Position Loop - Valid values include:
    • Disable & Coast
    • Current Decel & Disable
    • Current Decel & Hold
    • DC injection brake
    • AC injection brake
  • Velocity Loop - Valid values include:
    • Disable & Coast
    • Current Decel & Disable
    • Ramped Decel & Disable
    • Current Decel & Hold
    • Ramped Decel & Hold
    • DC injection brake
    • AC injection brake
  • Torque Loop - Valid values include:
    • Disable & Coast
    • Current Decel & Disable
    • Current Decel & Hold
    • DC injection brake
    • AC injection brake
Connection Loss Stopping Action
Specifies the stopping method applied to the motor when it detects a loss of connection.
The available options include:
  • Disable & Coast
  • Current Decel & Disable
  • Ramped Decel & Disable
  • Current Decel & Hold
  • Ramped Decel & Hold
Converter Input Phase Loss Action
Specifies the converter's response to an incoming phase loss while the converter is running.
The available options include:
  • Continue
  • Ride Thru
Power Loss Action
Specifies the power loss action for the motor.
Possible available options include:
  • Continue
  • Disable & Coast
  • Ramp Down
  • Ride Thru
Shutdown Action
Specifies the shutdown action of the motor.
The available options include:
  • Disable
  • Drop DC Bus
Motor Overload Action
Specifies the motor overload action for the motor.
The available options include:
  • <none>
  • Current Foldback
This field is optional.
Inverter Overload Action
Specifies the inverter overload action for the motor.
The available options include:
  • <none>
  • Current Foldback
This field is optional.
Drive Overload Action
Specifies the drive overload action for the motor.
The available options include:
  • <none>
  • Current Foldback
  • Reduce PWM Rate
  • PWM - Foldback
This field is optional.
AC Line Frequency Change Action
Specifies the converter's action when the rate of change of the AC line frequency exceeds a hard-coded threshold or the configured frequency change threshold.
  • Continue
  • Ride Thru
This field is optional for Regenerative Converters.
AC Line Sync Loss Action
Specifies the converter's response to an incoming line synchronization loss condition while the converter is running.
  • Continue
  • Ride Thru
AC Line Voltage Sag Action
Specifies the converter's response to an incoming AC Line Voltage Sag condition while the device is running.
  • Continue
  • Ride Thru
Converter Overload Action
Specifies the device's response to a converter overload condition.
  • None
  • Current Foldback
Parameters
Opens the
Motion Axis Parameters
page to modify existing or additional parameters.
Tip:
The
Parameter List
page may contain more attributes than the associated page. In some cases, attributes that display on the
Parameter List
page do not display on the associated page.
Danger: Vertical Load is enabled. Changing Action attributes from the Current Decel & Disable setting could endanger personnel, machine, and property.
Displays warning when
Vertical Load Control
setting on the
General
page is set to
Enabled
.
Safety Actions parameters
Parameter
Description
Safe Torque Off Action
Determines the stopping method to apply to the motor when the drive detects a Safe Torque Off (STO) Active condition that was not initiated by a Safe Stop 1 (SS1) Active condition, and
Safe Torque Off Action Source
is set to
Connected Drive
.
The available options include:
  • Disable & Coast
  • Current Decel & Disable
  • Ramped Decel & Disable
  • DC Injection Brake
  • AC Injection Brake
Safe Torque Off Action Source
Specifies whether the drive or the controller initiates the stopping sequence in response to a Safe Torque Off Active condition.
The available options include:
  • Connected Drive
    - the drive initiates the stopping sequence according to the Safety Torque Off Action selection
  • Running Controller
    - requires the user program to execute the stopping action
Safe Stopping Action
Specifies the stopping method that the drive is to apply to the motor. The available options include:
  • Current Decel
  • Ramped Decel
Safe Stopping Action Source
Specifies whether the drive or the controller initiates the stopping sequence in response to a Safe Stop Active condition.
The available options include:
  • Connected Drive
    - the drive initiates the stopping sequence according to the Safety Torque Off Action selection
  • Running Controller
    -
    requires the user program to execute the stopping action
Danger: Selection of Running Controller requires the user program to execute stopping action.
This warning displays when
Safe Stopping Action Source
or
Safe Torque Off Action Source
is set to
Running Controller
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal