Device Setup

The
Device setup
Tool allows you to discover and configure devices on a local network.
NOTE: In certain scenarios, the utilization of this Tool may be necessitated for the device registration to a domain. Furthermore, its behavior might differ depending on the device type and firmware version.

Stratix® 4300
featuring a firmware version older than or equal to 4.0.2

  1. Access
    FactoryTalk® Remote Access™
    Manager and select
    Tools
    Device setup
    .
  2. On the
    Device setup
    dialog window, select the first option:
    Stratix 4300 featuring a firmware version older than or equal to 4.0.2
    .
    NOTE: A pop-up message may appear asking for permission to open the Tool. Before confirming, you can check
    Always allow
    to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  3. In the dialog window, enter the
    Admin
    user's password.
    NOTE: These credentials are the same that you use to access the device System Manager, and the default password for an admin user is
    admin
    . To learn more about System Manager and to know the IP address that is used to access your device System Manager, download this user manual: Stratix 4300 router
    A new dialog window appears. It displays the MAC addresses of the routers in your local network that have a password matching the one specified.
  4. Select a router MAC address from the list and click
    Configure
    to set the LAN IP address. Then you can access the device System Manager to set up other parameters.

Stratix® 4300
featuring a firmware version newer than 4.0.2

  1. Access
    FactoryTalk® Remote Access™
    Manager and select
    Tools
    Device setup
    .
  2. On the
    Device setup
    dialog window, select the second option:
    Stratix 4300 featuring a firmware version newer than 4.0.2
    .
    NOTE: A pop-up message may appear which asks for permission to open the Tool. Before confirming, you can check
    Always allow
    to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  3. A discovery window appears. Select
    Discover
    to list all the devices on the local network that are in an
    Unconfigured
    state (factory default setting) or that were already configured.
    The
    Discovered devices
    list displays the
    Model
    ,
    Serial number
    ,
    Eth2:WAN IP address
    ,
    Eth1:LAN IP address
    and
    Status
    of each device.
  4. If you select the row of a device in an
    Unconfigured
    state, you can then open System Manager by selecting
    Device setup
    or set the IP address of a LAN interface, and restart.
    NOTE: To learn more about System Manager and to know the IP address that is used to access your device System Manager, download this user manual: Stratix 4300 router
    If you select the row of a device in a
    Configured
    state, you can open System Manager by selecting
    Device setup
    .

OptixPanel™ featuring a firmware version 4.0.4 or newer
,
Embedded Edge Compute Module featuring a firmware version 4.0.4 or newer
and
OptixEdge™

  1. Access
    FactoryTalk® Remote Access™
    Manager and select
    Tools
    Device setup
    .
  2. On the
    Device setup
    dialog window, select the third option:
    OptixPanel, OptixEdge or Embedded Edge Compute featuring a firmware version 4.0.4 or newer
    .
    NOTE: A pop-up message may appear which asks for permission to open the Tool. Before confirming, you can check
    Always allow
    to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  3. A discovery window appears. Select
    Discover
    to list all the devices on the local network that are in an
    Unconfigured
    state (factory default setting) or that were already configured.
    The
    Discovered devices
    list displays the
    Model
    ,
    Serial number
    ,
    Eth2:WAN IP address
    ,
    Eth1:LAN IP address
    and
    Status
    of each device.
  4. If you select the row of a device in an
    Unconfigured
    state, you can then open System Manager by selecting
    Device setup
    or set the IP address of a LAN interface, and restart.
    NOTE: To learn more about System Manager and to know the IP address that is used to access your device System Manager, download this user manual:
    If you select the row of a device in a
    Configured
    state, you can open System Manager by selecting
    Device setup
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal