Connection Settings

The advanced settings of connection ports and proxy server allow the Tool to connect to the
FactoryTalk® Remote Access™
network infrastrutture and establish a VPN connection with the remote device.
To configure network port and proxy settings for VPN connections:
  1. Access the
    FactoryTalk® Remote Access™
    Manager
    and select
    Tools
    Connection settings
    .
    NOTE: When clicking on
    Connection settings
    , a dialog window will show up asking for permission to open the
    Connection settings
    Tool. Prior to confirming, flag the
    Always allow
    checkbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
  2. Under
    Connection
    Port
    select the network port to use for VPN connections.
    • Auto:
      The Tool automatically selects the appropriate port based on the connection request.
    • 80:
      The Tool will only attempt to establish a remote access using the HTTP protocol over port 80. If the connection over port 80 is rejected, the session is not established.
    • 443:
      The Tool will only attempt to establish a remote access using the HTTP protocol over port 443. If the connection over port 443 is rejected, the session is not established.
    • 5935:
      The Tool will only attempt to establish a remote access using the HTTP protocol over port 5935. If the connection over port 5935 is rejected, the session is not established.
  3. If a proxy service is used for internet connections, select the type of proxy server under
    Proxy
    :
    • None:
      A proxy server is not used for the internet connection.
    • HTTP:
      HTTP Proxy Server. Forwards HTTP requests.
    • SOCKS5:
      SOCKS5 Proxy Server. Forwards TCP and UDP packets.
    NOTE: See Proxy for further information on this subject.
  4. After making your selections, click
    Apply
    to save the proxy settings to the domain.
Once the connection to the remote device is established, if the device is disconnected, it will enter a timeout mode while it automatically attempts to reconnect. In this situation, a warning icon displays while attempting to reconnect.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal