Validate a policy model
Validate a policy model to confirm that all devices are operational and have network access.
- From the toolbar, selectValidateand then select either:
- CIP protocolto validate connections betweenCIP Securitysystem components.
- OPC UA protocolto validate connections betweenOPC UAsystem components.
TIP: You can stop the validation process at any time by pressingSTOP VALIDATIONin the status bar.Resultsdisplays any potential warnings or errors. - (optional) Save the validation results by selecting.
Save
Provide Feedback