Delete a zone
Deleting a zone
removes all devices, conduits, and endpoints
assigned to the zone.Prerequisites
To retain the devices from the zone to delete, assign devices to different zones or unassign the devices from zones. If needed, recreate the conduits.
- To delete a zone
- From the navigation bar, select eitherCanvasorZones.TIP: InZONES, selectOverviewto see all zones in a table.
- Right-click the zone to delete and selectDelete.NOTE: To delete multiple zones, either:
- InZONES, hold, select multiple zones, and then selectCtrlnext to any selected zone.
Delete - InOverview, hold, select multiple zones, and then selectCtrlfrom the toolbar.
Delete
- SelectDELETE.
The zone is no longer a part of the policy model.
Provide Feedback