Delete a range
Delete a range of trusted IP addresses that you no longer need.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone that contains the range.
- SelectDevices.
- Right-click the range to delete and selectDelete.NOTE: To delete multiple ranges, hold, select multiple ranges, and then selectCtrlfrom the toolbar.
Delete - SelectDELETE.
The range is deleted and is no longer a part of the policy model.
Provide Feedback