Delete a port
Delete not needed ports from devices.
Prerequisites
Confirm that the device has more than one port configured.
- From the navigation bar, either:
- SelectCanvasand then select a device.
- SelectZonesand then select a zone and a device.
- SelectDevicesand then select a device.
- InProperties, underPorts, next to the port to delete, select.
Delete - SelectDELETE.
Provide Feedback