Configure a driver
A driver is the software interface to the computer or workstation hardware that allows the computer to communicate with a network to detect and communicate with a control system device.
- InDiscovery, on theCIPtab, select.
Configure Drivers - InConfigure Drivers:
- To configure a new driver, underAvailable Driver Types, select a driver, and selectAdd New.
- To edit a configured driver, next to the driver name, select.
Settings
- (optional) On theGeneraltab, assign a name for the device.
- UnderDiscovery Method, select either:
- Device List/Range. A discovery message is sent to each specified individual IP address. The list can identify target devices using the device name, IP address, or IP address range.
- Broadcast. A broadcast UDP message is sent to all devices on the network at once.
- InInterfaceselect the physical port of the computer.
- (optional) To listen on port 44818 and updateDiscoveryin response to network browse requests, selectListen on Ethernet/IP encapsulation ports.TIP: SelectingListen on Ethernet/IP encapsulation portsshows your computer in the network tree.
- SelectTuningand configure the tuning settings to change how fast items on the network are discovered.
- Device discovery poll rate (msec). Defines how often (in milliseconds) the Discovery pane requests data from a device. For example, a poll rate of 1000 ms results in data being requested every second. This setting is inactive when the driver uses broadcast discovery.TIP: When a driver makes a discovery request to a device, it waits for the amount of time specified by the Device discovery poll rate before making a request to a new device. Setting this rate to a higher value slows down the rate that devices appear in the browser tree, and reduces the number of messages sent on the network.
- Offline device discovery poll rate. Defines how often (in milliseconds) the Discovery pane waits to try to establish communication with an offline device. For example, a poll rate of 10,000 results in a 10-second delay before additional requests are sent to a device that was offline. This setting is inactive when the driver uses broadcast discovery.TIP: Setting this rate to a higher value slows down the rate that a newly attached device appears in the browser tree, and reduces the number of messages sent on the network.
- Poll interval between discovery cycles (msec). The number of milliseconds that occur between each query of the network by theDiscoverypane.TIP: After a driver polls the network branch, it waits the amount of time specified by the Poll Interval between discovery cycles before starting another discovery cycle. Setting the Poll interval between discovery cycles to a higher value reduces the number of network messages sent.
- Poll timeout (msec). Specifies the amount of time (in milliseconds) to wait for a device to respond to a request.
- Maximum concurrent packets to this network. Used to configure the maximum number of requests that can be waiting for a response on this network at any given time as part of the discovery process.
- (optional) SelectAuto remove offline devicesto hide offline devices fromDiscovery.
- SelectOK.
- SelectClose.
Provide Feedback