Bridge networks
Bridge networks to create conduits between networks.
- FromDiscovery, on theCIPtab, select.
Settings - On theBridgedtab, select+ Add New.
- InName, enter a name for the bridge.
- Next toSelected Target Bridge Network, selectBrowse.
- Either:
- To create a bridge path, inBridge Path Selection, select the network to connect the current network and then selectOK.
- To add an existing bridge path from another bridge, selectCopy Setting Fromand select a configuration.
- SelectOK.
Provide Feedback