Delete a device
Delete a not deployed device or a deployed device and its security configuration.
IMPORTANT:
If a device has multiple ports, the additional ports must be deleted to delete the device. Such devices are shown in the device table with the port name appended after the device name; for example,
Device3:Port2
If you delete a device from the proxy-proxied pair, both devices are deleted. The deleted device remains in the
Device
table until the next time the model is deployed. The properties of deleted devices are read-only.- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone.
- SelectDevices.
- Right-click the device to delete and selectDelete.NOTE: To delete multiple devices, inZonesorDevices, hold, select multiple devices, and then selectCtrlfrom the toolbar.
Delete - SelectDELETE.
- (deployed devices only) Deploy the policy model to clear the security policies from the deleted the device.For more information, see Policy model validation and deployment.
The device name and properties are struck-through. You cannot edit or assign deleted devices to the policy model.
To remove the device from the policy model and clear the device configuration, deploy the policy model. See Deploy a policy model.
Provide Feedback