Delete a conduit
Delete a conduit to remove a connection between two endpoints.
- From the navigation bar, selectConduits.
- Right-click the conduit to delete and selectDelete.NOTE: To delete multiple conduits, hold, select multiple conduits, and then selectCtrlfrom the toolbar.
Delete - SelectDELETE.
The conduit is no longer part of the policy model.
Provide Feedback