Add a conduit
Add a conduit to connect two endpoints. An endpoint can be either a device or a zone.
- From the navigation bar, either:
- SelectCanvasand then select from the toolbar.TIP: You can also right-click a zone, device, or range and then selectAdd Conduit.
- SelectConduitsand then selectAddfrom the toolbar.
- InCONDUIT PROPERTIES, underEndpoint 1, select.

- Select a zone or device to assign as the first endpoint of the conduit and selectOK.TIP: UseFilterto find endpoints.
- UnderEndpoint 2, select.

- Select a zone or device to assign as the second endpoint of the conduit and selectOK.
- SelectNext.
- Make changes inCONDUIT PROPERTIES.For more information, see Conduit properties.
Provide Feedback