Policy model example
The policy model example includes three zones connected with conduits that contain different device types.
Policy model example

Item | Name | Description |
|---|---|---|
![]() | CIP and OPC UA zone | Contains OPC UA devices and CIP devices. |
![]() | Secure conduit | Connects CIP and OPC UA zone with OPC UA zone. |
![]() | Trusted unsecure conduit | Connects OPC UA zone with CIP Security zone. |
![]() | OPC UA zone | Contains OPC UA devices only, including two OPC UA clients and one OPC UA server. |
![]() | CIP Security zone | Contains three CIP devices. |
![]() | Onboarding Area container | Contains devices found by Automatic Policy Deployment that can be added to the policy model. There are no devices found by Automatic Policy Deployment in this example. |
![]() | Unassigned container | Contains devices added to the policy model but not added to any zone in the policy model. There are two unassigned devices in this example. |
Provide Feedback