Merging
Depending on the policy model and the devices available in the network, the merging process can be automatic or manual.
Automatic merging
The merging process is automatic if the onboarding device has the same IP address as the matching device in the policy model.
The onboarding device does not need to be identical with the matching device in the policy model. During the merging process, the newer device properties overwrite the older device properties.
TIP:
The following properties are never overwritten by the automatic merging process:
- IP address
- Device name
- Device description
The following tables illustrate the examples on how the automatic merging process operates in different scenarios.
Onboarding device | Device in the policy model (Zone 1) | Merged device (Zone 1) | Description |
|---|---|---|---|
IP Address: 192.168.1.68 Name: 1756-L81E Description: 1756-L81E Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN12345 | IP Address: 192.168.1.68 Name: Line Controller Description: Main controller for assembly line Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN12345 | IP Address: 192.168.1.68 Name: Line Controller Description: Main controller for assembly line Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN12345 | All device parameters match:
The device malfunctioned and was reset to factory defaults. |
Onboarding device | Device in the policy model (Zone 1) | Merged device (Zone 1) | Description |
|---|---|---|---|
IP Address: 192.168.1.68 Name: 1756-L81E Description: 1756-L81E Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN12345 | IP Address: 192.168.1.68 Name: Line Controller Description: Main controller for assembly line Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN54321 | IP Address: 192.168.1.68 Name: Line Controller Description: Main controller for assembly line Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN1234 | All device parameters match except for:
The device malfunctioned and was replaced with a new device. |
Onboarding device | Device in the policy model (Zone 2) | Merged device (Zone 2) | Description |
|---|---|---|---|
IP Address: 192.168.1.73 Name: 1756-L83E Description: 1756-L83E Product type: 14 Product code: 166 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN111213 | IP Address: 192.168.1.73 Name: Machine Controller Description: Packaging machine controller Product type: 14 Product code: 166 Firmware major revision: 33 Firmware minor revision: 001 Serial number: SN313211 | IP Address: 192.168.1.73 Name: Machine Controller Description: Packaging machine controller Product type: 14 Product code: 166 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN111213 | All device parameters match except for:
The device malfunctioned and was replaced with a new device. |
Onboarding device | Device in the policy model (Zone 3) | Merged device (Zone 3) | Description |
|---|---|---|---|
IP Address: 192.168.1.82 Name: 1756-EN4TR Description: 1756-EN4TR Product type: 12 Product code: 258 Firmware major revision: 4 Firmware minor revision: 001 Serial number: SN223344 | IP Address: 192.168.1.82 Name: Conveyor PF755T #12 Description: Conveyor drive #12 Product type: 45 Product code: 7 Firmware major revision: 10 Firmware minor revision: 00 Serial number: SN556677 | IP Address: 192.168.1.82 Name: Conveyor PF755T #12 Description: Conveyor drive #12 Product type: 12 Product code: 258 Firmware major revision: 4 Firmware minor revision: 001 Serial number: SN223344 | A non-typical scenario with device mismatch. The existing device is treated as obsolete and overwritten. The device parameters are merged:
|
Manual merging
The merging process is manual if the onboarding device cannot be associated with any device in the policy model.
An administrator can manually move the discovered device from the Onboarding Area to the policy model.
The following table illustrates an example of the manual merging process.
Onboarding device | Device in the policy model | Merged device | Description |
|---|---|---|---|
IP address: 192.168.1.68 Name: 1756-L81E Description: 1756-L81E Product type: 14 Product code: 164 Firmware major revision: 34 Firmware minor revision: 001 Serial number: SN12345 | No match | N/A | No matching device found in the policy model. Device added to the Onboarding Area. |
Provide Feedback