Purchase a FactoryTalk Optix Studio Pro entitlement

FactoryTalk® Optix™
Studio Pro is available by subscription only. Purchase and allocate or assign an entitlement to an organization in order to activate
FactoryTalk® Optix™
Studio Pro. You must have a purchase order to purchase software.
Devices that are not activated operate in demo mode and stop running
FactoryTalk® Optix™
applications after 2 hours. The
Emulator
client that runs
FactoryTalk® Optix™
applications on the development computer does not require a runtime entitlement.
  1. From the Commerce Portal, log in to your MyRockwellAutomation account.
  2. Scroll to
    FactoryTalk® Optix™
    and under
    FactoryTalk® Optix™
    , select
    Continue
    .
  3. Select your package, scroll to select options to customize your package, and then under
    Select Quantity
    , select the number of entitlements.
  4. Select
    ADD TO CART
    . You can change the number of entitlements in your cart.
    TIP: If you copied a
    FactoryTalk® Optix™
    Runtime catalog number from the Runtime Sizing tool, you can paste the selected catalog number in the search bar at the top of the Commerce Portal page. Paste the catalog and select to add the catalog number to your cart.
  5. Review your cart and the pricing with your Distributor and then select
    CHECKOUT
    .
  6. Confirm your shipping, billing, contract details, and order summary and then select
    SUBMIT ORDER
    .
  7. On the confirmation page, select
    Manage Licenses
    and confirm your new contract.
Once the entitlement status is active, the entitlement appears in FactoryTalk Hub. You can also confirm your order status in the Commerce Portal by selecting
My Subscriptions/Manage Licenses
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal