Allocate a FactoryTalk Optix Studio Pro entitlement to your organization

A newly purchased entitlement can be viewed by the purchaser in
FactoryTalk® Hub™
. Then, the entitlement must be allocated to the related organization, to be made available to other users as well.
  1. Access FactoryTalkHub.com to view your new entitlement.
  2. In the
    FactoryTalk® Hub™
    page title bar, select , then select
    View Entitlements
    .
    This image shows where to find View Entitlements in the menu of FactoryTalk
              Hub.
    The new entitlement appears at the top of
    All entitlements
    under
    Available for allocation
    .
  3. Verify that the correct organization name appears on the right side of the
    FactoryTalk® Hub™
    title bar.
  4. Locate the entitlement that you want to assign to your organization and select
    Allocate
    next to the entitlement row.
    This image shows where to allocate an available entitlement in FactoryTalk
              Hub.
  5. Ensure that the entitlement, organization and allocated entitlements quantity are correct, then select
    Allocate
    .
    This image shows where to click to allocate an entitlement.
    IMPORTANT: Once allocated to an organization, an entitlement cannot be deallocated.
  6. In the upper left corner of the
    FactoryTalk® Hub™
    web page, select
    Home
    .
  7. Select the
    FactoryTalk Optix
    tile.
    Select the FactoryTalk Hub to access the FactoryTalk Optix webpage.
  8. At the top of the
    FactoryTalk® Optix™
    landing page, select
    Entitlements
    .
  9. On the
    Entitlements
    page, select
    Organization entitlements
    .
The allocated entitlement appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal