NuGet packages

Some library widgets and scripts require specific NuGet packages to be installed.
For more information about NuGet, see What is NuGet and what does it do? | Microsoft Docs.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 6.0 destination framework.
Install NuGet packages in the code editor of your choice. See Install NuGet packages in Visual Studio and Install NuGet packages in Visual Studio Code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal