Project encryption

Encrypt projects on
Windows®
client devices and
OptixPanel
.

Encryption scope

Project
YAML
files, which represent the project information model, are transferred as encrypted binary files on client devices. For more information, see Project source format.
By default, Emulator components are encrypted. You cannot disable the encryption of Emulator components.

Public encryption key

Client devices generate public encryption keys based on the current hardware and
Windows
keys. The public encryption keys in
EncryptionKey.bin
are stored on the client devices in the
Runtime
folder.
Encrypted projects cannot be copied to or run on different client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal