Create a local project

Create a local project with version control to create the local project and a local repository on your computer. The local repository allows you to commit changes to your project and provides version control to view and restore previous versions of your project.
  1. If there is an open
    FactoryTalk Optix
    project, select
    Project
    and then select
    Close Project
    .
  2. Select
    Close
    or if there are changes to save, select
    Save and close
    .
  3. On the Start page, select
    New
    .
  4. Select the type of project.
  5. In
    Name
    , enter the name of the project.
    TIP: The project and repository names must be the same, including capitalization.
  6. In
    Location
    , type the path to the project.
  7. Select
    Use version control
    .
    TIP: When version control is enabled for a local project and you want to back up the project to a remote repository, push the local changes to associate the local project with a remote repository.
  8. Select
    Create
    .
Version control is added to the new project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal