Display variables

Bind a property of a graphic object to a predefined
Display
variable to configure the screen of the HMI device. For example, bind to the
Brightness
variable to specify the brightness level of the display of the HMI device. To bind to a variable, see Create dynamic links.
The
Display
category in the Dynamic Link browser displays the variables related to the HMI device screen.
Display variables
Variable
Type
Definition
Read or Write
Reboot Required
Brightness
UInt32
Display brightness of the HMI device screen (1-10)
Read/Write
Reboot not required
Vertical resolution
UInt32
Vertical resolution of the HMI device display in pixels
Read-only
Reboot not required
Horizontal resolution
UInt32
Horizontal resolution of the HMI device display in pixels
Ready-only
Reboot not required
Scale
UInt32
Zoom level of the display (50-200)
Read/Write
Reboot required
Orientation
UInt32
Orientation of the display:
1 = Landscape
2 = Portrait
3 = Portrait flipped
Read/Write
Reboot required
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal