Duplicate a project

Duplicate a project to use an existing project as a template for a new project.
  1. Open the project to be copied and then from the main menu, select
    Save as
    .
  2. In
    Save project as
    , complete:
    1. Name
      . The name of the new project.
    2. Location
      . The storage location of the project files. The duplicated project is stored in the same location as the original project by default. Select the folder icon to browse to a new location.
    3. (optional)
      Use Source Control
      . Select to save your project in a Git repository.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal