Set the unit of measure for a variable

Set the unit of measurement for a numeric figure.
  1. In
    Project view
    , select a variable.
  2. In
    Properties
    , right-click the numeric variable name and select
    New
    EUInformation
    .
  3. Select the unit of measure for the variable value and choose
    Select
    .
The unit of measure appears in the value for the variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal