Push Agent interface

The example Push Agent UI contains five variables, a data grid with associated buttons, and fields that allow you to configure the data logger.
TIP:
Download a sample project:
PushAgentDemo.zip
The sample project includes a Push Agent that is configured to connect to an Eclipse Mosquitto broker locally and uses these third-party NuGet packages:
  • MqttNet
  • Newtonsoft.Json
Push Agent UI Example
The example of the Push Agent UI contains the following elements:
Callout
Item
Description
A
Data grid
Illustrates the samples detected by the data logger based on the selected mode, which you can change in the drop-down menu.
B
Refresh button
Updates the data grid.
C
Log button
Inserts a row with the values of the sampled variables into the data grid.
D
Data logger configuration section
Enables you to modify the configuration parameters of the monitored variables and the data logger. To send data to the cloud, you must configure all parameters related to the broker.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal