Apply a global style to the project

Select a style sheet for a
FactoryTalk Optix Application
to display at runtime.
Prerequisites
  1. To apply a global style to the project
  2. In
    Project view
    , select either
    NativePresentationEngine
    or
    WebPresentationEngine
    .
  3. In
    Properties
    , in
    Style sheet
    , select the drop-down arrow after the style sheet value and then select the style sheet to apply.
The project uses the
Global Style
properties from the selected style sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal